Camera module for i.MX 6SoloX sabre evalboard

cancel
Showing results for 
Search instead for 
Did you mean: 

Camera module for i.MX 6SoloX sabre evalboard

158 Views
markus_willbol1
Contributor I

Hello,

I´m searching for a camera module for our evalboard MCIMX6SX-SDB (see attachment). Connector J13 has a 40 pin interface.
My problem is, that I don´t find a camera on the market that fits to the connector J13.

Is there a module available on the market?

I want to use the parallel interface of the camera interface
A pin description of J13 would also be interesting.

Thanks!

Best regards

Markus

Labels (2)
0 Kudos
1 Reply

79 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Markus Willbold,

This board is designed so the Omnivision OV5640/5642 5M Pixel Sensor is used.

The cameras part number and distributor can be found on the following thread:

https://community.nxp.com/message/314081?commentID=314081#comment-314081

“The cameras on the boards come from Omnivision (Ordering Number: OV05640-MRFL-AA0T) and can be ordered through distributor Nu Horizons”.

Although availability may vary. I hope this helps!

Regards,

0 Kudos