Camera for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Camera for i.MX6

850 Views
1990rahulreddy
Contributor IV

I am new to i.MX6 board. I have to use MIPI camera for i.MX6 SABRESDP. please provide link from where i can buy & tutorial for it to install.

Thanks in Advance

Labels (2)
3 Replies

570 Views
art
NXP Employee
NXP Employee

The i.MX6 SABRE SDP board comes already equipped with the MIPI camera OV5640. All required drivers are included in the Board Support Packages (BSPs), provided by Freescale (check the "Board Support Packages" section):

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

570 Views
1990rahulreddy
Contributor IV

I didnt get answer to my question from last two days. Where I can find this

On Thu, Sep 17, 2015 at 9:58 AM, b45499 <admin@community.freescale.com>

0 Kudos

570 Views
saurabh206
Senior Contributor III

Hi
Rahul

i.MX6 SABRESDP board comes with MIPI camera support.

Connected MIPI camera is OV5640.

http://boundarydevices.com/product/nit6x_5mp_mipi/

For implementation you can go through following link

Integration Support for ov5645 camera over mipi-csi2 interface

I hope this helps.

Thanks

Saurabh