Camera display is abnormal imx8m min

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Camera display is abnormal imx8m min

791件の閲覧回数
Andrew_yang
Contributor II

Hi,

I porting a camera with MIPI CSI interface on the imx8m min platform Android9.0, Camera display is abnormal, When turn on the camera, I can preview it at the beginning, But it gets stuck pretty quickly.

When preview, Display very laggard and print log as below from mx6s_capture.c  

When preview be stuck,No kernel log print.

*************************************

[ 839.891085] skip frame 1
[ 840.171775] skip frame 0
[ 840.331090] skip frame 0
[ 840.412334] skip frame 0
[ 840.491342] skip frame 0
[ 841.091180] skip frame 1
[ 841.291117] skip frame 1
[ 841.571235] skip frame 0
[ 841.651498] skip frame 0

**********************************

Can you help to provide some solutions advices ?  Thanks !

 

ラベル(3)
0 件の賞賛
返信
0 返答(返信)