Camera capture at same time through IC and directly to memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Camera capture at same time through IC and directly to memory

1,362 Views
erezsteinberg
Contributor IV

Dear experts,

I am wondering if the following is possible.

iMX6 is connected to a single CMOS sensor, e.g. 1080p.

Is it possible to have both paths working at the same time:

CSI -> MEM

CSI -> IC -> MEM

So, for every frame, I can get the original image from the sensor (CSI->MEM)  + a downscaled image (CSI->IC->MEM) ?

Can iMX6 support such a configuration in theory?

Sincerely,

Erez

Labels (1)
0 Kudos
Reply
1 Reply

1,226 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Basically it is possible (to have the both paths working at the same time).

According to section 37.4.3.1 (CSI Block Diagram) of the i.MX6 DQ Reference Manual :

“The CSI gets data from the sensor […] and transfer it according to configuration of DATA_DEST

register to one or more of the following: IC, SMFC.” Bit field DATA_DEST allows setting both
destination IC and SMFC simultaneously. Please take a look at section 37.5.151 [CSI0 Sensor
Configuration Register (IPUx_CSI0_SENS_CONF)] 

Nevertheless, I am afraid, practically it is not simple job to implement this approach, since

in any case finally AXI bus (via IDMAC) is destination for all data. You may look at Figure 37-1

(IPU Block Diagram) and Figure 37-2 (IPU Detailed Block Diagram).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply