Camera Issue in Android Marshmallow 6.0.1 in imx6 sabresd Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Camera Issue in Android Marshmallow 6.0.1 in imx6 sabresd Board

784 Views
lakshmikanthr
Contributor III

I have ported Android Marshmallow 6.0.1 into imx6 sabresd Board and flash the image to Board. I'm facing camera problem , couldn't open the camera.

 

Please find the attachment of CTS failure list. Hope do you have any idea. Please consider my request to solve my problem.

Original Attachment has been moved to: host_log_4493427107813570818.zip

Original Attachment has been moved to: device_logcat_6619181058126652047.zip

Labels (1)
0 Kudos
4 Replies

582 Views
lakshmikanthr
Contributor III

Hi,

Thank you for responding mail.

Usually, I had followed that same reference documents only.  

i.e android_M6.0.1_2.1.0_docs.tar.gz

can you help me , how to solve the problem ?

Thanks & Regards,

Lakshmikanth

0 Kudos

582 Views
diegoadrian
NXP Employee
NXP Employee

Which camera are you using?

0 Kudos

582 Views
lakshmikanthr
Contributor III

Hi,

Thank you for reply.

The Board contains inbuilt camera i.e ( MIPI camera) . Unable to open the camera.

Thanks & Regrads,

Lakshmikanth R

0 Kudos

582 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Do you are using out BSP? This is because our BSP normally support the use of the cammer.

If not, try building the Android image with our BSP.

In the below link, you can find the Android documentation and BSP.

Android OS for i.MX Applications Processors|NXP 

Best Regards,

Diego.

0 Kudos