CVBS output on i.MX6q(with adv7393)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CVBS output on i.MX6q(with adv7393)

1,576 Views
hyunhoshin
Contributor III

I'm using custom made imx6q board(with adv7393 CVBS output only)

I'm already patch BT656 output(https://community.freescale.com/docs/DOC-94019)

so, CVBS output(NTSC) work fine.

some monitor work fine. but, some monitor can't display

not work case, adv7393 SD timing mode set to master mode(self generating timing) and then it could display the screen(timing is not match)

(how to master mode change : adv7393 register 0x8A set to 0x9-default value is 0x8)

i think h/v timing value issue.

help me please...

thank you.

P.S. My source version L3.0.35_1.1.0

Labels (3)
0 Kudos
Reply
3 Replies

841 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Shin  ,

    Questions on ADV7393, please contact ADI company !

    In addition, The MAX clock of CSI on i.MX6 can't be more than 240MHz, check it , please !

Regards,

Weidong

0 Kudos
Reply

841 Views
hyunhoshin
Contributor III

ADV7393 is TV encoder(CVBS out)

ADV7393's color bar pattern(self generated) display is nomal for all monitors

but iMX6's BT656 signal though ADV7393 is not display on some monitors(not all)

0 Kudos
Reply

841 Views
art
NXP Employee
NXP Employee

Most likely, some (non-working in your case) monitors just do not support the resolution of a frame the i.MX6 outputs through CVBS. Please check.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply