CSI1 data port selection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CSI1 data port selection

Jump to solution
1,152 Views
johnciple
Contributor I

Hi,

I am designing with iMX6D.

I have to connect the CSI1 and parallel Camera(8bit bayer).

EIM Ports have IPU2_CSI1_DATA0 ~ IPU2_CSI1_DATA19.

Can I select data port?

I want to use IPU2_CSI1_DATA10 ~ IPU2_CSI1_DATA17.

Because I want to avoid to overlap with BootConfig.

Is this OK?

Labels (1)
0 Kudos
Reply
1 Solution
999 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please use section 4.11.10.1 (IPU Sensor Interface Signal Mapping)

of the Datasheet about supported CSI signals connections.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,000 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please use section 4.11.10.1 (IPU Sensor Interface Signal Mapping)

of the Datasheet about supported CSI signals connections.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply