CSI0 test mode does not work with input channel CSI->IC->MEM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CSI0 test mode does not work with input channel CSI->IC->MEM

1,133件の閲覧回数
RobbieJiang
Contributor IV

Hi,

I would like to have CSI0 work in test mode on my Mx6q sabrelite board.

But by now, I can only capture data through input channel 1, that is ,

from CSI directly to memory.  And no data can be captured through input channel 0,

which is CSI-->IC-->MEM.

So does csi in test mode  only work with input channel CSI-->MEM?

ラベル(2)
0 件の賞賛
返信
1 返信

956件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what test mode do you mean? if you mean the unit test, mxc_v4l2_capture.out is for csi-> mem, mxc_v4l2_overlay.out is for Direct previewing the camera to SDC foreground

0 件の賞賛
返信