CRUX-ARM running on EfikaMX Smarttop -blog archive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CRUX-ARM running on EfikaMX Smarttop -blog archive

832 Views
VictorMartinez
Contributor I

CRUX-ARM [1] now supports EfikaMX Smarttop device (iMX51).

Current version is 2.7. There is a documentation webpage [2] where we try to put all the info related to these devices together.

 

Current working on:

- HardFP ABI currently built and tested [3] (working right but without much feedback to put more hands on)

- Provide an installation method based on a SD card to install CRUX-ARM directly in the SSD.

- CRUX-ARM 2.7.1 version update (based on native builds instead of cross-compilations)

  - One generic (softfp) release without optimizations and probably another one with armv7 optimizations for EfikaMX

  - Another HardFP release optimized for EfikaMX devices. 

 

CRUX-ARM community can be found here [4]. There are some resources like a irc channel in freenode and a mailing list.

Currently there are two videos (poor quality) to show EfikaMX boot time into a login manager (around 1 minute) and another one which shows Enlightenment (DR17) start/load time and performance. They can be found here [5]

 

[1] http://crux-arm.nu

[2] http://crux-arm.nu/SupportedDevices/EfikaMX-SmartTop

[3] http://crux-arm.nu/files/devices/efikamx/hardfp/

[4] http://crux-arm.nu/Main/Community

[5] http://crux-arm.nu/files/videos/

Tags (1)
0 Kudos
Reply
0 Replies