CRC check failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CRC check failed

937件の閲覧回数
niharunadkat
Contributor I

Hi,

I am using kernel version 4.1.18 for ARM processor 32bit.

The kernel reside and boots up from eMMC.

After about 10 reboot Consequently

I get the following error

fdt: not creating '/sys/firmware/fdt': CRC check failed
Waiting for root device /dev/mmcblk0p2...

What does this error mean? And how do I resolve this issue.

Any help and suggestion would greatly be appreciated.

Thank you

Nihar

0 件の賞賛
2 返答(返信)

824件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Nihar,

This command is used for deployment a NFS file system using TFTP connection. Do you use a Network File system?

Is there problem if booting from the SD card is used?

Regards

0 件の賞賛

824件の閲覧回数
niharunadkat
Contributor I

Hello,

I tried the same test in the SD card and it has not failed. It works all the time.

With eMMC Linux boot 90% of the time. When Linux fails it hangs at "Waiting for root device /dev/mmcblk0p2...". U-boot is always successful.

0 件の賞賛