Board - imx6 Sabre for smart device
OS - Yocto linux 4.9.88 .
Problem - When i run QT demo application , top command shows CPU load around 70% . QT5 app is using GPU as shown by gpuinfo.sh
top - 17:37:55 up 4:45, 1 user, load average: 0.30, 0.07, 0.02
Tasks: 151 total, 1 running, 150 sleeping, 0 stopped, 0 zombie
%Cpu(s): 13.8 us, 17.3 sy, 0.0 ni, 68.9 id, 0.0 wa, 0.0 hi, 0.0 si, 0.0 st
KiB Mem : 1024200 total, 680760 free, 236468 used, 106972 buff/cache
KiB Swap: 0 total, 0 free, 0 used. 692108 avail Mem
PID USER PR NI VIRT RES SHR S %CPU %MEM TIME+ COMMAND
2684 root 20 0 240940 45152 24512 S 74.0 4.4 0:10.88 Qt5_NMap_C+
641 root 20 0 183408 18352 10284 S 43.8 1.8 0:07.56 weston
2627 root 20 0 0 0 0 S 4.3 0.0 0:41.70 kworker/0:0
255 root 20 0 0 0 0 S 2.3 0.0 0:00.54 galcore de+
2689 root 20 0 3256 1872 1520 R 1.6 0.2 0:00.22 top
1 root 20 0 24544 5484 4492 S 0.0 0.5 0:07.59 systemd
2 root 20 0 0 0 0 S 0.0 0.0 0:00.02 kthreadd
3 root 20 0 0 0 0 S 0.0 0.0 0:00.02 ksoftirqd/0
5 root 0 -20 0 0 0 S 0.0 0.0 0:00.00 kworker/0:+
7 root 20 0 0 0 0 S 0.0 0.0 0:00.39 rcu_preempt
8 root 20 0 0 0 0 S 0.0 0.0 0:00.00 rcu_sched
9 root 20 0 0 0 0 S 0.0 0.0 0:00.00 rcu_bh
10 root rt 0 0 0 0 S 0.0 0.0 0:00.01 migration/0
11 root 0 -20 0 0 0 S 0.0 0.0 0:00.00 lru-add-dr+
12 root 20 0 0 0 0 S 0.0 0.0 0:00.00 cpuhp/0
13 root 20 0 0 0 0 S 0.0 0.0 0:00.00 cpuhp/1
14 root rt 0 0 0 0 S 0.0 0.0 0:00.01 migration/1
CPU load is quite bad (170%) with qtwebengine (quicknanobrowser) running a simple html which is rendering few straight lines .
Can you please help , how to increase GPU performance so that it does not use CPU much ?
On kernel startup , i can see only two logs for vivante driver intialisation -
[ 1.492125] [drm] Initialized
[ 1.494324] [drm] Initialized vivante 1.0.0 20120216 on minor 0
Does yocto for imx6 support etnaviv driver ?
Is high CPU usage shows , some problem with the GPU driver ??