CPU failed to boot : Error with 3.14.28 kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CPU failed to boot : Error with 3.14.28 kernel

ソリューションへジャンプ
3,241件の閲覧回数
sharvari
Contributor I

Hello all,

  I am facing issue with linux-imx 3.14.28 kernel. I have a imx6solo sabre auto based board.

When I flash the kernel generated from Yocto (meta-fsl-arm), it gives the following error

-----------------------------------------------------------------------------------------------------------------------------------------

Virtual kernel memory layout:

  vector : 0xffff0000 - 0xffff1000 ( 4 kB)

  fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)

  vmalloc : 0xa0800000 - 0xff000000 (1512 MB)

  lowmem : 0x80000000 - 0xa0000000 ( 512 MB)

  pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)

  modules : 0x7f000000 - 0x7fe00000 ( 14 MB)

  .text : 0x80008000 - 0x806d54ac (6966 kB)

  .init : 0x806d6000 - 0x80a6a100 (3665 kB)

  .data : 0x80a6c000 - 0x80aaa1e0 ( 249 kB)

  .bss : 0x80aaa1ec - 0x80b0cc20 ( 395 kB)

*SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1*

Preemptible hierarchical RCU implementation.

  RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.

RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2

NR_IRQS:16 nr_irqs:16 16

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32050000, Cache size: 512 kB

failed to set parent of clk gpu2d_core_sel to pll2_pfd1_594m: -22

Switching to timer-based delay loop

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every

1431655765682ns

Console: colour dummy device 80x30

Calibrating delay loop (skipped) preset value.. 1581.05 BogoMIPS

(lpj=7905280)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)

Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x10516040 - 0x10516098

*CPU1: failed to boot: -38*

Brought up 1 CPUs

SMP: Total of 1 processors activated.

------------------------------------------------------------------------------------------------------------------------------------------

My board is solo, but the kernel debug messages show CPUs =2.

Also it gives error as CPU1:failed to boot. Do i need to change any

configurations in Yocto or kernel config to make CPUS=1?

-Thanks

Sharvari

ラベル(4)
0 件の賞賛
返信
1 解決策
2,258件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Sharvari

you are right, for Solo one needs to use kernel boot parameter

maxcpus=1 or nosmp

Also recommend to look at attached Linux Guide sect.5 Enabling Solo Emulation

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,259件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Sharvari

you are right, for Solo one needs to use kernel boot parameter

maxcpus=1 or nosmp

Also recommend to look at attached Linux Guide sect.5 Enabling Solo Emulation

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,258件の閲覧回数
sharvari
Contributor I

Thanks igor.

I added nosmp to kernel boot parameter and it worked.

-Thanks

Sharvari Harisangam

0 件の賞賛
返信