CPU频率调整

cancel
Showing results for 
Search instead for 
Did you mean: 

CPU频率调整

531 Views
1182614726
Contributor III

大家好,

              使用的芯片为imx6solo,BSP为yocto L4.1.15-2.1.0.

              目前在uboot运行的时候,发现CPU运行在792MHz,请问如何设置可以让CPU运行在最高主频996MHz,

              非常感谢NXP各位大神帮忙支持,谢谢。

Labels (1)
0 Kudos
1 Reply

435 Views
radhikasomaiya
Senior Contributor II

Hi qiang xie,

Checkout this thread. Let us know in case of any query regarding this.

Regards,

Radhika

0 Kudos