Hi Guys,
Thanks to this blog.
http://imxcv.blogspot.ca/2014/02/building-opencv-24x-for-freescales-imx6.html
I added it onto conf/local.conf
CORE_IMAGE_EXTRA_INSTALL += " gpu-viv-bin-mx6q gpu-viv-bin-mx6q-dev "
and run bitbake fsl-image-qt5 but faced these errors..
ERROR: Nothing RPROVIDES 'gpu-viv-bin-mx6q' (but /home/smart/yocto/var-som-mx6-yocto-jethro/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-qt5.bb RDEPENDS on or otherwise requires it)
NOTE: Runtime target 'gpu-viv-bin-mx6q' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['gpu-viv-bin-mx6q']
ERROR: Required build target 'fsl-image-qt5' has no buildable providers.
Missing or unbuildable dependency chain was: ['fsl-image-qt5', 'gpu-viv-bin-mx6q']
Question:
1. Doesn't YOCTO support "gpu-viv-bin-mx6q gpu-viv-bin-mx6q-dev" anymore? if yes, How can I add viv-bin?
2. Whenever I face such kind of errors, What should I see to know whether some images are available in YOTO today or not?
One of difficulty to use YOCTO is that
there are a lot of different config names like below..
EXTRA_IMAGE_FEATURES =
IMAGE_INSTALL_append =
PACKAGECONFIG_append_pn-qtbase =
CORE_IMAGE_EXTRA_INSTALL =
but, I don't know exactly what image or receipes need to be appended on which config name above..
I have red YOCTO mega manual but it doesn't give all the information about the configs
for instance, I can't find PACKAGECONFIG_append_pn-qtbase in mega manual but it is needed to append linuxfb with QT.
Hi hj.,
gpu_viv debian packages are no longer available. Looks like you are using a older bsp version, please try the latest one:
i.MX6Q|i.MX 6Quad Processors|Quad Core|NXP
and you try to read the user guide document for reference about differnets backend images that the bsp provides.
Hope this helps