CLK1 and CLK2 enable in i.MX8M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLK1 and CLK2 enable in i.MX8M

1,907件の閲覧回数
yashavanthashet
Contributor V

Hi,

Kindly let us know how to enable CLK1 and CLK2 (CCM instance) coming from CPU in Linux kernel.

We are using i.MX8M custom board with Linux4.9.51_ga release.

Thanks in advance.

Regards,

Yashavantha

4 返答(返信)

1,687件の閲覧回数
art
NXP Employee
NXP Employee

The CLK1_P/N and CLK2_P/N differential clock signals are intended to be used for internal/factory test purposes only. They should not be used for regular operation.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,687件の閲覧回数
yashavanthashet
Contributor V

Hi Arut,

Thank you for the reply.

We are not intended to use CLK1 and CLK2 for regular operation, just we wanted to check whether its enabled or not.

When we probe the respective pins we are not getting any clock pulse. So we wanted to enable it, if it is not enabled.

Best Regards,

Yashavantha

0 件の賞賛
返信

1,687件の閲覧回数
art
NXP Employee
NXP Employee

As I told before, this is not required for normal operation. CLK1_P/N is the debug clock input only, and the CLK2_P/N debug clock output is disabled by default.

Best Regards,

Artur

1,687件の閲覧回数
plentod
Contributor I

Artur,

The IMX8M HW Dev Guide (IMX8MDQLQHDG, section 3.9) talks about using CLK2 as a source for the PCIe interface (when not using an external clock generator).  Can CLK2 still be enabled as a 100MHz ref clk for this purpose?  If so, is there an updated ref manual/app_note that describes how to configure/enable CLK2 output?

Thanks, David Plentovich

0 件の賞賛
返信