CHANNEL_SELECT field when i.MX6 is set to eCSPI slave mode.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CHANNEL_SELECT field when i.MX6 is set to eCSPI slave mode.

ソリューションへジャンプ
1,635件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 eCSPI.

I understand that CHANEL_SELECT field in ECSPIxCONREG register is set when i.MX6 is master mode and communicates with a external slave device.

Then, I want to confirm whether CHANNEL_SELECT field is also set in i.MX6DQ is eCSPI slave mode or not.

Would you let me know it?

Best Regards,

Satoshi Shimoda

タグ(1)
0 件の賞賛
返信
1 解決策
1,443件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The CHANNEL_SELECT field cannot be used to get the SS status.

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,443件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  According to section 21.4.2 (Slave Mode) of the i.MX6 D/Q RM :

"In this configuration, Chip Select (SS) becomes an input signal, and is used to control

data transfers through the Shift register, as well as to load/store the data FIFO."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,443件の閲覧回数
satoshishimoda
Senior Contributor I

Dear Yuri,

Did you mean "we can confirm whether SS is input to i.MX6 or not by reading CHANNEL_MODE field"?

Or in slave mode, SS status is not affected to CHANNEL_MODE?

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
1,444件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The CHANNEL_SELECT field cannot be used to get the SS status.

Regards,

Yuri.

0 件の賞賛
返信