Hi All,
I wonder if there is any additional step needed to set GPIO1_IO5 pad to CCM_CLKO1 output
I can easly set it for GPIO1_IO0 as this is its default location, but also i can set it simultanously on CSI0_HSYNC pad (ALT3), but not on GPIO1_IO05.
I've verified both settings for CCM module registers and IOMUX registers, but still no joy
I've also verified that i acually have control over GPIO1_IO5 pad setting it into GPIO mode and driving it manually, also i've tested my settings on another hardware to exclude any hardware malfunction - as i said, with no luck.
Anyways, if someone could point me in right direction i would apreciate it. for this point i'm assuming this is imx6 core bug
Please advise
Best regards,
Sebastian