CCM_CLK1_P clock output 8MHz generating settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CCM_CLK1_P clock output 8MHz generating settings

1,642件の閲覧回数
prabhu1
Contributor III

Hi man/sir,

I am using i.mx6ull processor I need to generate 8MHz clock output in pin P17(CCM_CLK1_P), pls can u help how to generate a clock from i.mx6ull (settings in internal processor).

0 件の賞賛
返信
3 返答(返信)

1,497件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi prabhu

allowable options are described in sect.18.7.18 Miscellaneous Register 1 (CCM_ANALOG_MISC1n) 

i.MX6ULL  RM, seems there is no 8MHz option.

http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,497件の閲覧回数
velayutha_perum
Contributor I

Hi Igorpadykov,

          I need to generate 26MHz clock output in pin P17(CCM_CLK1_P), pls can u help how to generate a clock from i.mx6ull (settings in internal processor). Do you know which register is used to configure this PIN ?

0 件の賞賛
返信

1,497件の閲覧回数
prabhu1
Contributor III

Hi Igorpadykov,

Thanks for the reply, but I want to get the clock in CCM_CLK1_P pin expecting 8MHz clock (p17 pin i.mx6ull) what changes (any exact registers & dividers in inside processor) or from 24Mhz external clock source how to get 8Mhz clock inside processor? and connections between CCM_CLK1_P pin(p17) & 24Mhz clock inside IC ?

0 件の賞賛
返信