CCM_CBCMR register value not at default indicated in data-sheet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CCM_CBCMR register value not at default indicated in data-sheet

Jump to solution
1,470 Views
ts
Contributor II

Hi,

We're trying to bring up a new i.mx6q design and using DS-5 over jtag.  The CCM_CBCMR (0x020c4018) register value observed is always 0x004A0324 and not 0x00022324 as indicated in data sheet.

Does the boot-rom modify default register values or is there some other setting (e.g. efuses) that we need to look at to know why our register values don't match defaults?

thanks,

Tarak

Labels (1)
1 Solution
1,375 Views
Yuri
NXP Employee
NXP Employee

Yes, the boot ROM can change clock settings, using fuse parameters, please look at section 8.4.3 (Clocks at Boot Time)
and section 8.3.1 (Boot eFUSE Descriptions) of the i.MX6Q Reference Manual.

View solution in original post

1 Reply
1,376 Views
Yuri
NXP Employee
NXP Employee

Yes, the boot ROM can change clock settings, using fuse parameters, please look at section 8.4.3 (Clocks at Boot Time)
and section 8.3.1 (Boot eFUSE Descriptions) of the i.MX6Q Reference Manual.