CAN1 TX Interrupt triggered continously [imx287cv]

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN1 TX Interrupt triggered continously [imx287cv]

953 次查看
hrishikesh23
Contributor I

Hi,

We have ported linux :

Linux CMS5 2.6.35.3-670-g914558e-svn1803 #43 PREEMPT Wed Mar 19 12:01:03 IST 2014 armv5tejl GNU/Linux.

We have initially Enabled cano interface and tested which works fine. Later we moved on to enable can1 interface. But eventually we are facing problems with can1 when there is no device connected to the bus.

can1 interrupts keeps on increamenting with count of 1000 per sec.

root@ ~$ cat /proc/interrupts  [J

           CPU0

  6:          0           -  pswitch

  8:         18           -  can0

  9:    2013315           -  can1

38:          0           -  fb_irq

39:          0           -  mxs-pxp

this is the register dump for both can interfaces .

root@ ~$ cat /sys/devices/platform/FlexCAN.0/dump_reg

MCR::0x4087023f

CTRL::0x2a4e0c4

RXGMASK::0x0

RX14MASK::0x0

RX15MASK::0x0

ECR::0x0

ESR::0x30

IMASK2::0xffffffff

IMASK1::0xffffffff

IFLAG2::0x0

IFLAG1::0x0

root@ ~$

root@~$ cat /sys/devices/platform/FlexCAN.1/dump_reg

MCR::0x4087023f

CTRL::0x2a4e0c4

RXGMASK::0x0

RX14MASK::0x0

RX15MASK::0x0

ECR::0x80

ESR::0x250

IMASK2::0xffffffff

IMASK1::0xffffffff

IFLAG2::0x0

IFLAG1::0x0

BUS STATE :


root@ ~$ cat /sys/devices/platform/FlexCAN.1/state
Start::error passive

root@ ~$ cat /sys/devices/platform/FlexCAN.0/state
Start::bus off

can 0 comes back from Bus off state to normal state but this behaviour is not observe in case of can1.

also i found that my loopback bit is set in CTRL register. which probably dont need to be set ? Please suggest me regarding this.

should i enable the AEN bit MCR register ? what all bits should be enabled if this configuration has to enabled ?

Please suggest. thanks in advance .

Message was edited by: hrishikesh choudhary

标签 (2)
0 项奖励
回复
0 回复数