As suggested, we checked the lib/modules folder. No CAN related files found. We checked in vendor folder.
We have used both pre built as well as builded image. In both case no can device is found.
Also, there is no CAN related logs in kernel.
Then we updated the dts files as attached.(open using text viewer)
Now we are getting following logs in boot(attached logs):
can-stby : disabling
can-en : disabling
How can we add the CAN modules and where to find the related files?
Also, if there is any android automotive pre-built that supports CAN, please share the link. We have tried in 12.1.0_1.1.0.
We also tried running Linux 5.4.70_2.3.0(just to check if CAN is working) , the board is not starting with the files available.