CAN/UART communication in MIMXRT1170 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN/UART communication in MIMXRT1170 EVK

1,239 Views
AnweshaPanda
NXP Employee
NXP Employee

I want to send data from 1170 EVK to another microcontroller, hence wanted to understand the internal connection to the CAN transreceiver on the evaluation board. is there any available examples  or demo program in sdk depository. Any hardware or jumper modification required to achieve the CAN communication. Any documentation in this regard will also be of help. 

0 Kudos
Reply
1 Reply

1,231 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you refer to the attachment to learn the board setting for CAN communication.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply