CAN 0 node is not appeared when we build flexcan driver along with kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN 0 node is not appeared when we build flexcan driver along with kernel

1,395 次查看
santhoshkarthik
Contributor III

Hi,

   CAN 0 node is not appeared(in ifconfig -a) when we built along with kernel and I could not do following commands

$echo 125000 > /sys/devices/platform/FlexCAN.0/bitrate

$ip link set can0 up

But if we build FlexCAN as a module, It works and I appiled following patch as well

linux-2.6.35.3-imx28/flexCAN-fixes.patch at master · embeddedarm/linux-2.6.35.3-imx28 · GitHub

Please help me to resolve this issue.

Thanks,

Karthik

标签 (1)
0 项奖励
回复
0 回复数