CAAM support on imx6sl-evk board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAAM support on imx6sl-evk board

Jump to solution
1,066 Views
sandeepajesh
Contributor III

Hi Experts,

Do we have Linux CAAM driver support on imx6sl-evk board , as I can not see any entry in .dts file. Please help. 

Regards

Sandeep S

Labels (1)
1 Solution
843 Views
art
NXP Employee
NXP Employee

The i.MX6SoloLite processor does not contain the CAAM module in its SoC hardware by its design, so, there is no CAAM support in software for it.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
844 Views
art
NXP Employee
NXP Employee

The i.MX6SoloLite processor does not contain the CAAM module in its SoC hardware by its design, so, there is no CAAM support in software for it.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

843 Views
sandeepajesh
Contributor III

Thanks Artur,

Thanks a lot for your response.  

Artur ,We want to use RNG hardware module available on imx6sl for our use-case. Currently we trying with below changes:-

Kernel Flags enabled:-

CONFIG_HW_RANDOM=y

CONFIG_HAVE_IMX_RNG=y

            CONFIG_HW_RANDOM_IMX_RNG=y

 

Device Tree:-

rng: rng@021b4000 {

                compatible = "fsl,imx6sl-rng", "fsl,imx-rng", "imx-rng";

                reg = <0x021b4000 0x4000>;

                interrupts = <0 5 IRQ_TYPE_LEVEL_HIGH>;

                clocks = <&clks IMX6SL_CLK_DUMMY>;

            };

Then we are going to use rngtest to testing purpose. Please let me know if I am missing something here.

Regards

Sandeep S

0 Kudos
Reply