CAAM support from within OP-TEE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CAAM support from within OP-TEE

跳至解决方案
1,850 次查看
matthias_staube
Contributor II

Dear Yuri,

I am interested in CAAM support from within OP-TEE as well. I see that there seems to be some support through core/drivers/caam, but I am not sure. Could you send me the information as well? I am using i.MX 8MQuad. Thank you in advance!

Best Regards,

Matthias

1 解答
1,666 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 By default,Cryptographic algorithms are not accelerated by CAAM on OPTEE.

To get more details, please create  request (case \ ticket) for it.

   

Support | NXP 


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

在原帖中查看解决方案

2 回复数
1,667 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 By default,Cryptographic algorithms are not accelerated by CAAM on OPTEE.

To get more details, please create  request (case \ ticket) for it.

   

Support | NXP 


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

1,666 次查看
matthias_staube
Contributor II

Hello Yuri,

I created a ticket as requested:

Case:00242494:CAAM acceleration within OP-TEE OS

Thank you for your support!

Kind Regards,

Matthias