CAAM Black Blob Implementation on i.MX8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAAM Black Blob Implementation on i.MX8

Jump to solution
5,592 Views
kile964
Contributor II

Hello,

I'm following the i.MX Linux Users Guide  document and trying to implement CAAM black blob functionality. The guide refers to the caam-keygen utility, which doesn't seem to be included in the community BSP. I found this utility instead here

If I compile and run on the processor, I get the following error:

Unable to open device /dev/caam-keygen

 Otherwise, I get successful results for all the checks listed in the guide:

# grep -B1 -A2 tk /proc/crypto
name : tk(ecb(aes))
driver : tk-ecb-aes-caam
module : kernel
priority : 1
--

name : tk(cbc(aes))
driver : tk-cbc-aes-caam
module : kernel
priority : 1

# dmsetup targets
crypt v1.19.0
striped v1.6.0
linear v1.4.0
error v1.5.0

Processor is IMX8MM. I'm using Yocto dunfell (boundary devices BSP). I have added all of the packages recommended in the guide docs and I believe all kernel configuration parameters are enabled correctly.

 # zcat /proc/config.gz | grep CAAM
CONFIG_CRYPTO_DEV_FSL_CAAM_DMA=y
CONFIG_CRYPTO_DEV_FSL_CAAM_COMMON=y
CONFIG_CRYPTO_DEV_FSL_CAAM_CRYPTO_API_DESC=y
CONFIG_CRYPTO_DEV_FSL_CAAM_AHASH_API_DESC=y
CONFIG_CRYPTO_DEV_FSL_CAAM_SECVIO=y
CONFIG_CRYPTO_DEV_FSL_CAAM=y
CONFIG_CRYPTO_DEV_FSL_CAAM_DEBUG=y
CONFIG_CRYPTO_DEV_FSL_CAAM_JR=y
CONFIG_CRYPTO_DEV_FSL_CAAM_RINGSIZE=9
CONFIG_CRYPTO_DEV_FSL_CAAM_INTC=y
CONFIG_CRYPTO_DEV_FSL_CAAM_INTC_COUNT_THLD=255
CONFIG_CRYPTO_DEV_FSL_CAAM_INTC_TIME_THLD=2048
CONFIG_CRYPTO_DEV_FSL_CAAM_CRYPTO_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_AHASH_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_PKC_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_RNG_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_TK_API=y
# CONFIG_CRYPTO_DEV_FSL_CAAM_RNG_TEST is not set
CONFIG_CRYPTO_DEV_FSL_CAAM_SM=y
CONFIG_CRYPTO_DEV_FSL_CAAM_SM_SLOTSIZE=7
# CONFIG_CRYPTO_DEV_FSL_CAAM_SM_TEST is not set
CONFIG_CRYPTO_DEV_FSL_CAAM_JR_UIO=y

 

0 Kudos
1 Solution
5,494 Views
kile964
Contributor II

I, too, am building a boundary devices bsp, though I was on kernel 5.4.70. After some back and forth with them, they showed me how to source the latest boundary-imx (AKA linux-boundary) kernel from 5.4.80 which includes the /dev/caam-keygen node. This isn't yet included in the official dunfell release.

Here's the recipe - changes to latest dunfell release are bold.

# Adapted from linux-imx.inc, copyright (C) 2013, 2014 O.S. Systems Software LTDA
# Released under the MIT license (see COPYING.MIT for the terms)

require recipes-kernel/linux/linux-imx.inc

SUMMARY = "Linux kernel for Boundary Devices boards"

LICENSE = "GPLv2"
LIC_FILES_CHKSUM = "file://COPYING;md5=bbea815ee2795b2f4230826c0c6b8814"

LINUX_VERSION = "5.4.80"

SRC_URI = "git://github.com/boundarydevices/linux-imx6.git;branch=${SRCBRANCH} \
"

LOCALVERSION = "-2.2.0-ga+yocto"
SRCBRANCH = "boundary-imx_5.4.x_2.2.0"
SRCREV = "38b03360c36c606656c65d9128d3cd29ea0ce6d6"
DEPENDS += "lzop-native bc-native"
COMPATIBLE_MACHINE = "(nitrogen6x|nitrogen6x-lite|nitrogen6sx|nitrogen7|nitrogen8m|nitrogen8mm|nitrogen8mn)"

KBUILD_DEFCONFIG ?= "boundary_defconfig"

S = "${WORKDIR}/git"

"../sources/meta-freescale-3rdparty/recipes-kernel/linux/linux-boundary_5.4.bb" 24L, 780C

 

 

View solution in original post

6 Replies
5,526 Views
a_1359
Contributor II

@Yuri 

Hello,

I am also facing the same problem on an iMX6D platform:

 

~# caam-keygen create randomkey ecb -s 16
Unable to open device /dev/caam-keygen

 

 

Running the following kernel version on the target from boundaydevices:

 

# uname -r
4.14.98-2.0.0_ga+yocto+gde875982909f

 

 

with the following configs:

 

# zcat /proc/config.gz | grep -i caam                                                                                        
CONFIG_CRYPTO_DEV_FSL_CAAM=y
CONFIG_CRYPTO_DEV_FSL_CAAM_JR=y
CONFIG_CRYPTO_DEV_FSL_CAAM_RINGSIZE=9
# CONFIG_CRYPTO_DEV_FSL_CAAM_INTC is not set
CONFIG_CRYPTO_DEV_FSL_CAAM_CRYPTO_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_AHASH_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_PKC_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_RNG_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_TK_API=y
# CONFIG_CRYPTO_DEV_FSL_CAAM_RNG_TEST is not set
CONFIG_CRYPTO_DEV_FSL_CAAM_SM=y
CONFIG_CRYPTO_DEV_FSL_CAAM_SM_SLOTSIZE=7
# CONFIG_CRYPTO_DEV_FSL_CAAM_SM_TEST is not set
# CONFIG_CRYPTO_DEV_FSL_CAAM_SECVIO is not set
# CONFIG_CRYPTO_DEV_FSL_CAAM_DEBUG is not set
CONFIG_CRYPTO_DEV_FSL_CAAM_CRYPTO_API_DESC=y
CONFIG_CRYPTO_DEV_FSL_CAAM_AHASH_API_DESC=y

 

  

However, I do not have the ./dev/caam-keygen node as mentioned in the docs:

 

# cd /; find -name "caam-keygen" 
./usr/bin/caam-keygen

 

 

Your feedback is appreciated!

Regards,

a_1359

0 Kudos
5,495 Views
kile964
Contributor II

I, too, am building a boundary devices bsp, though I was on kernel 5.4.70. After some back and forth with them, they showed me how to source the latest boundary-imx (AKA linux-boundary) kernel from 5.4.80 which includes the /dev/caam-keygen node. This isn't yet included in the official dunfell release.

Here's the recipe - changes to latest dunfell release are bold.

# Adapted from linux-imx.inc, copyright (C) 2013, 2014 O.S. Systems Software LTDA
# Released under the MIT license (see COPYING.MIT for the terms)

require recipes-kernel/linux/linux-imx.inc

SUMMARY = "Linux kernel for Boundary Devices boards"

LICENSE = "GPLv2"
LIC_FILES_CHKSUM = "file://COPYING;md5=bbea815ee2795b2f4230826c0c6b8814"

LINUX_VERSION = "5.4.80"

SRC_URI = "git://github.com/boundarydevices/linux-imx6.git;branch=${SRCBRANCH} \
"

LOCALVERSION = "-2.2.0-ga+yocto"
SRCBRANCH = "boundary-imx_5.4.x_2.2.0"
SRCREV = "38b03360c36c606656c65d9128d3cd29ea0ce6d6"
DEPENDS += "lzop-native bc-native"
COMPATIBLE_MACHINE = "(nitrogen6x|nitrogen6x-lite|nitrogen6sx|nitrogen7|nitrogen8m|nitrogen8mm|nitrogen8mn)"

KBUILD_DEFCONFIG ?= "boundary_defconfig"

S = "${WORKDIR}/git"

"../sources/meta-freescale-3rdparty/recipes-kernel/linux/linux-boundary_5.4.bb" 24L, 780C

 

 

5,570 Views
Yuri
NXP Employee
NXP Employee

@kile964 
Hello,

  Use AN12714 (i.MX Encrypted Storage Using CAAM Secure Keys):

https://www.nxp.com/docs/en/application-note/AN12714.pdf

  Also: AN12554 (Demo Application to Generate Red/Black Blobs Using CAAM
                            and Encrypt/Decrypt Data)

https://www.nxp.com/docs/en/application-note/AN12554.pdf

  The recent app note - hope - will be updated soon.

Regards,
Yuri.

0 Kudos
5,540 Views
kile964
Contributor II

Hi Yuri,

Can you help me understand what provides /dev/caam-keygen ? I'm working with the same kernel version (5.4.47) as AN12714 with seemingly the same list of packages.

Thank you.

0 Kudos
5,553 Views
a_1359
Contributor II

@Yuri 

could you please let me know why my message is deleted in this post?

I have got it working right now! but really wondering how my post including only and only pure technical stuff should be deleted in this post.
I believe that in NXP community forum people should treat each other with mutual respect.
I am disappointed about this but happy that I have got it working on my platform without any support in just couple of hours:
 

a_1359_0-1607631394185.png

 

Regards,

a_1359

0 Kudos
5,532 Views
a_1359
Contributor II

Hi,

Which kernel version you are using on your target?

The link of the keyctl_caam that you have posted i.e. https://source.codeaurora.org/external/imx/keyctl_caam/?h=imx_5.4.47_2.2.0 is on 5.4.47 branch!


Problems can happen due to the Linux kernel API mismatches, I mean the kernel that you are running and the kernel that keyctl_caam has been written for.

If this is the case, then it would be wise to compile the keyctl_caam from a branch that matches your Linux kernel version. However, I am not sure that this can be the problem!

The other point is that there is apparently just one single branch on the keyctl_caam i.e. 5.4.47. So it seems this should not be the problem.

I am facing the same problem on i.MX6D. I am running kernel 4.14.98 from boundarydevices.

# caam-keygen create randomkey ecb -s 16
Unable to open device /dev/caam-keygen

# cd /; find -name "caam-keygen"
./usr/bin/caam-keygen

And the doc says:

root@imx8mmevk:~# cd /; find -name "caam-keygen"

./usr/bin/caam-keygen

./dev/caam-keygen

./sys/class/misc/caam-keygen

./sys/devices/virtual/misc/caam-keygen

 

Obviously, I am missing ./dev/caam-keygen node! but why ?!

 

Regards,

a_1359