Bypass USB VBUS detection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bypass USB VBUS detection

2,889 次查看
danielenderle
Contributor II

By design we cannot use OTG_VBUS Pin to detect if imx6 is connected as slave to a host machine. 

Is there a way to get USB OTG Slave mode working without using VBUS detection?

We are running Android 6.0.1/Linux 4.1.15.

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

2,412 次查看
danielenderle
Contributor II

Hi Igor

i tried to find similiar source files where i can patch your suggested link but without any success.

Can you lead me to find the destination where i can patch those files for imx6?

Best regards

Daniel

0 项奖励
回复

2,412 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

may be helpful

I.MX6 : Using USB OTG without dynamic VBUS pin ? 

Best regards
igor

0 项奖励
回复

2,412 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

one can try to use similar patch for i.MX28

USB Device not work when VDD5V is not attached during boot (iMX28) 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复