Bypass USB VBUS detection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bypass USB VBUS detection

2,900 Views
danielenderle
Contributor II

By design we cannot use OTG_VBUS Pin to detect if imx6 is connected as slave to a host machine. 

Is there a way to get USB OTG Slave mode working without using VBUS detection?

We are running Android 6.0.1/Linux 4.1.15.

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,423 Views
danielenderle
Contributor II

Hi Igor

i tried to find similiar source files where i can patch your suggested link but without any success.

Can you lead me to find the destination where i can patch those files for imx6?

Best regards

Daniel

0 Kudos
Reply

2,423 Views
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

may be helpful

I.MX6 : Using USB OTG without dynamic VBUS pin ? 

Best regards
igor

0 Kudos
Reply

2,423 Views
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

one can try to use similar patch for i.MX28

USB Device not work when VDD5V is not attached during boot (iMX28) 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply