Busfreq OPTEE set from 24000000 to 400000000 start.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Busfreq OPTEE set from 24000000 to 400000000 start.

跳至解决方案
1,916 次查看
layleon
Contributor III

There is a lot of this information that will always be displayed periodically, why? How to mute it? Can I only modify the source code without printk? 

[  206.247131] Busfreq OPTEE set from 400000000 to 24000000 start...
[  206.255946] Busfreq OPTEE set to 24000000 done! cpu=0
[  206.295989]
[  206.295989] Busfreq OPTEE set from 24000000 to 400000000 start...
[  206.332122] Busfreq OPTEE set to 400000000 done! cpu=0
[  209.447133]
[  209.447133] Busfreq OPTEE set from 400000000 to 24000000 start...
[  209.455924] Busfreq OPTEE set to 24000000 done! cpu=0
[  209.496017]
[  209.496017] Busfreq OPTEE set from 24000000 to 400000000 start...
[  209.532123] Busfreq OPTEE set to 400000000 done! cpu=0
[  212.647100]
[  212.647100] Busfreq OPTEE set from 400000000 to 24000000 start...
[  212.655921] Busfreq OPTEE set to 24000000 done! cpu=0
[  212.696172]
[  212.696172] Busfreq OPTEE set from 24000000 to 400000000 start...
[  212.732340] Busfreq OPTEE set to 400000000 done! cpu=0
[  215.847153]
[  215.847153] Busfreq OPTEE set from 400000000 to 24000000 start...
[  215.855952] Busfreq OPTEE set to 24000000 done! cpu=0
[  215.895905]
[  215.895905] Busfreq OPTEE set from 24000000 to 400000000 start...
[  215.931981] Busfreq OPTEE set to 400000000 done! cpu=0
[  219.047116]
[  219.047116] Busfreq OPTEE set from 400000000 to 24000000 start...
[  219.055954] Busfreq OPTEE set to 24000000 done! cpu=0
[  219.115985]
[  219.115985] Busfreq OPTEE set from 24000000 to 400000000 start...
[  219.141949] Busfreq OPTEE set to 400000000 done! cpu=0
[  222.727073]
[  222.727073] Busfreq OPTEE set from 400000000 to 24000000 start...
[  222.735873] Busfreq OPTEE set to 24000000 done! cpu=0
[  222.775976]
[  222.775976] Busfreq OPTEE set from 24000000 to 400000000 start...
[  222.812075] Busfreq OPTEE set to 400000000 done! cpu=0
[  225.927155]
[  225.927155] Busfreq OPTEE set from 400000000 to 24000000 start...
[  225.935970] Busfreq OPTEE set to 24000000 done! cpu=0
[  225.975879]
[  225.975879] Busfreq OPTEE set from 24000000 to 400000000 start...
[  226.012141] Busfreq OPTEE set to 400000000 done! cpu=0
[  229.127121]
[  229.127121] Busfreq OPTEE set from 400000000 to 24000000 start...
[  229.135966] Busfreq OPTEE set to 24000000 done! cpu=0
[  229.176856]
[  229.176856] Busfreq OPTEE set from 24000000 to 400000000 start...
[  229.212407] Busfreq OPTEE set to 400000000 done! cpu=0
[  232.487115]
[  232.487115] Busfreq OPTEE set from 400000000 to 24000000 start...
[  232.495906] Busfreq OPTEE set to 24000000 done! cpu=0
[  232.536256]
[  232.536256] Busfreq OPTEE set from 24000000 to 400000000 start...
[  232.571992] Busfreq OPTEE set to 400000000 done! cpu=0
[  235.687101]
[  235.687101] Busfreq OPTEE set from 400000000 to 24000000 start...
[  235.695880] Busfreq OPTEE set to 24000000 done! cpu=0
[  235.754748]
[  235.754748] Busfreq OPTEE set from 24000000 to 400000000 start...
[  235.781876] Busfreq OPTEE set to 400000000 done! cpu=0

 

0 项奖励
回复
1 解答
1,871 次查看
igorpadykov
NXP Employee
NXP Employee

one can look at sect.2.5.4 Dynamic Bus Frequency  i.MX Linux Reference Manual​

so if voltages are fixed, busfreq driver may be disabled. Depending on processor load voltages may

vary as "fsl,soc-operating-points" show in dts

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6ull.dtsi?h=imx_5.4.4...

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
6 回复数
1,902 次查看
igorpadykov
NXP Employee
NXP Employee

Hi layleon

 

what processor and bsp used in the case. Is it possible to reproduce issue on some nxp

reference board with demo images from:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 项奖励
回复
1,899 次查看
layleon
Contributor III

BSP:5.4.47_2.2.0​​

Self-designed hardware, using IMX6UL.

Boot from NAND.

微信截图_20201210174408.png

0 项奖励
回复
1,884 次查看
igorpadykov
NXP Employee
NXP Employee

"Self-designed hardware" - uses pmic or based on nxp i.MX6UL EVK reference design ?

 

Best regards
igor

0 项奖励
回复
1,880 次查看
layleon
Contributor III

fixed 3V3/1V2/1V35 by DC-DC converter

The same DDR P/N, 128MB NAND, has been booted and the DDR has been calibrated.

Reading the code, it looks like the DDR frequency keeps changing(periodicity) from 24MHz to 400MHz(400MHz to 24MHz), which triggers this change, why is this? This output is very disturbing to debug ah.

 

微信截图_20201210220008.png

 

微信截图_20201210215903.png

0 项奖励
回复
1,872 次查看
igorpadykov
NXP Employee
NXP Employee

one can look at sect.2.5.4 Dynamic Bus Frequency  i.MX Linux Reference Manual​

so if voltages are fixed, busfreq driver may be disabled. Depending on processor load voltages may

vary as "fsl,soc-operating-points" show in dts

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6ull.dtsi?h=imx_5.4.4...

 

Best regards
igor

0 项奖励
回复
1,861 次查看
layleon
Contributor III

Example Patch,both the kernel(linux-imx) and the bootloder(u-boot) need to be patched.

 

diff --git a/arch/arm/boot/dts/imx6ul.dtsi b/arch/arm/boot/dts/imx6ul.dtsi
index 3a9985cb0dd9..e0809eabf4ff 100644
--- a/arch/arm/boot/dts/imx6ul.dtsi
+++ b/arch/arm/boot/dts/imx6ul.dtsi
@@ -59,22 +59,16 @@
 			compatible = "arm,cortex-a7";
 			device_type = "cpu";
 			reg = <0>;
-			clock-frequency = <696000000>;
+			clock-frequency = <528000000>;
 			clock-latency = <61036>; /* two CLK32 periods */
 			#cooling-cells = <2>;
 			operating-points = <
 				/* kHz	uV */
-				696000	1275000
 				528000	1175000
-				396000	1025000
-				198000	950000
 			>;
 			fsl,soc-operating-points = <
 				/* KHz	uV */
-				696000	1275000
 				528000	1175000
-				396000	1175000
-				198000	1175000
 			>;
 			clocks = <&clks IMX6UL_CLK_ARM>,
 				 <&clks IMX6UL_CLK_PLL2_BUS>,

 

0 项奖励
回复