From Datasheet IMX8DXAEC Rev2:
"Keeper Circuit Resistance" is defined only single-voltage GPIO port.
But, It seems that we can select bus-keeper setting on following balls via PULL field in pad configuration register.
USB_SS3_TC0
USB_SS3_TC1
USB_SS3_TC2
USB_SS3_TC3
ADC_IN0
ADC_IN1
ADC_IN2
ADC_IN3
ADC_IN4
ADC_IN5
SCU_WDOG_OUT
PMIC_I2C_SCL
PMIC_I2C_SDA
PMIC_INT_B
SCU_BOOT_MODE0
SCU_BOOT_MODE1
SCU_BOOT_MODE2
SCU_BOOT_MODE3
MIPI_CSI0_MCLK_OUT
MIPI_CSI0_I2C0_SCL
MIPI_CSI0_I2C0_SDA
MIPI_CSI0_GPIO0_01
MIPI_CSI0_GPIO0_00
SCU_PMIC_STANDBY
SCU_GPIO0_00
SCU_GPIO0_01
<Questions>
Q1. Which balls support bus-keeper function? Is it only support above balls?
Q2. The bus-keeper feature is only applied for GPIO input mode. Is it right?
Q3. The bus-keeper feature does not mentioned in the current RM. Will it be revised in the nearly future?
Best Regards,
Kazuma Sasaki.
解決済! 解決策の投稿を見る。
Hello,
Use the following resource for more details about i.MX8 pin configuration.
System Controller Firmware 101 - Pad configuration service
As for the questions:
1) yes, only the pins having the PULL bit field with bus-keeper option support bus-keeper function;
2) only inputs have bus-keeper option;
3) there is no information about documentation details.
Regards,
Yuri.
Hello,
Use the following resource for more details about i.MX8 pin configuration.
System Controller Firmware 101 - Pad configuration service
As for the questions:
1) yes, only the pins having the PULL bit field with bus-keeper option support bus-keeper function;
2) only inputs have bus-keeper option;
3) there is no information about documentation details.
Regards,
Yuri.
Dear Yuri,
I appreciate your support. Your explanation really helped.
Best Regards,
Kazuma Sasaki.