I know that U-Boot can write the fuses, but how is this done from UUU? I have searched the UUU PDF file, and the word "fuse" does not occur in the document.
This suggests that it is possible (see #2):
Looking at the UUU document, Table 2, SDP should be used with i.MX6. UUU documentation does not mention "+FB". So what is the difference between FB and +FB? Is +FB valid for the i.MX6?
From Burning_eFuses_on_i.MX8_and_i.MX8x_families:
SDPS: boot -f imx-boot-imx8qxpmek-sd.bin-flash
+FB: ucmd fuse prog -y 0 708 0xa295fc11
+FB: ucmd fuse prog -y 0 709 0x000017b4
FB: ucmd setenv fastboot_dev mmc
Hi JohnKlug
in general uuu is using uboot with fastboot, for example fuse usage one can look at
https://imxdev.gitlab.io/tutorial/Burning_eFuses_on_i.MX8_and_i.MX8x_families/
Best regards
igor