Built YOCTO on IMX6,error:version of patch is older than 2.7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Built YOCTO on IMX6,error:version of patch is older than 2.7

686 Views
mengsuma
Contributor I

When I built YOCTO on IMX6, after running the bitbake fsl-image-validation-imx code, I got the following error:

topeet@ubuntu:~/fsl-release-bsp/build-x11$ bitbake fsl-image-validation-imxERROR: OE-core's config sanity checker detected a potential misconfiguration.
Either fix the cause of this error or at your own risk disable the checker (see sanity.conf).
Following is the list of potential problems / advisories:

Your version of patch is older than 2.7 and has bugs which will break builds. Please install a newer version of patch.


Summary: There was 1 ERROR message shown, returning a non-zero exit code.

I don't know what this "patch" is

0 Kudos
Reply
2 Replies

610 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello ma,

You need run yocto in ubuntu 16.04 to eliminate this issue since your are using pypl whit less than 2.0 version.

Regards

610 Views
mengsuma
Contributor I
Thanks, this is useful
8/5000
Thanks, this is useful
0 Kudos
Reply