Buildroot2014.05 download failure of xserver-xorg-video-imx-viv 3.5.7-1.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Buildroot2014.05 download failure of xserver-xorg-video-imx-viv 3.5.7-1.0.0

909 Views
andreaszeiler
Contributor III

Hello,

i have a problem when building my rootfs in buildroot 2014.05.

when buildroot is downloading the packages the files have the size of 0bytes. so i think they were not downloaded.

my mirror is :

FREESCALE_IMX_VERSION = 3.5.7-1.0.0

FREESCALE_IMX_SITE    = http://www.freescale.com/lgfiles/NMG/MAD/YOCTO/

or

FREESCALE_IMX_VERSION = 3.0.35-4.0.0

# No official download site from freescale, just this mirror

FREESCALE_IMX_MIRROR_SITE   = http://download.ossystems.com.br/bsp/freescale/source

is there another mirror where I can download the files with buildroot? i can search for the files and  i already have some of them but this is no solution because the mirrors have to be right when customers want to build buildroot ...

regards andi

0 Kudos
Reply
1 Reply

675 Views
gusarambula
NXP TechSupport
NXP TechSupport

Unfortunately these mirror does not seem to be part of the official Community BSP. Maybe some user which used these files can tell us if they were replaced.


Perhaps the following document might help:

Setup Xorg 1.14 for i.MX6

0 Kudos
Reply