Building yocto project has a problem and downloading was failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Building yocto project has a problem and downloading was failed

969 次查看
tangyuan
Contributor III

HI,

    All,i am building a yocto project accord the document .1.jpg

    But i do the step,it was failed

    here is the step?:

    2.jpg

       When i do the repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.28-1.0.0.ga,it report the error

       3.jpg

        Similarly,i do the step :4.jpg

        curl http://commondataastorage.googleapis.com/git-repo-downloads/repo  >~/bin/repo

        It report the error:5.jpg

      Can anyone help me?

                                                                                                                                                                                                THANKS

0 项奖励
回复
1 回复

870 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Tang Yuan,

Please make sure that you have internet access. In case you’re using a proxy please check your settings. Building the Yocto BSP requires an active internet connection at all times in order to download metadata and fetch the source code. 

Regards,

0 项奖励
回复