Hi,
need help to deal with following situation:
I have generated new configuration file for above mentioned Kernel version but i don't know why nothing is changed when i try to run it on board. I just followed instructions in Freescale_Yocto_User_Guide section(5.6.7), but i suppose they are not valid for this kernel version somehow 3.10.53. Can anyone guide me out of this problem?
Thanking in advance.
Best regards,
Faisal
Please look at recommendations below how to change the kernel configuration
through menuconfig
$ bitbake -c menuconfig linux-imx
This creates a config file in (as an example)
tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.0.35-r33.10/git/.config
This file should be copied to the defconfig location in order to set the changes.
Below is an example of the devconfig location :
meta-fsl-arm/recipes-kernel/linux/linux-imx-3.0.35/mx6
Then use the commands.
$ bitbake -c cleansstate linux-imx
$ bitbake linux-imx
As for configuring the kernel more details are available on the following community document:
https://community.freescale.com/docs/DOC-95045
Regards,
Yuri.
Thanks for the reply. Just wanna point out in your case your kernel version is different from mine. And problem with new kernel is it's defconfig files are directly fetched from package and build. My assumption is either you need to apply it through patch file (new yocto layer) or you need to workaround in your build folder with git/arch/arm/configs/imx_v7_deconfig file. Now the real issue if you replace this default defconfig with your new defconfig and do the process of clean state and build. The defconfig is automatically replaced by default configuration.