Building keras and tensor flow on yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Building keras and tensor flow on yocto

2,978 次查看
jarviscrypter
Contributor I

I have been trying to build keras and tensor flow packages on yocto's image that is poky but not able to do so.

Until now I have tried looking for their respective recipe but couldn't find.
What's the way to add keras and tensor flow packages to poky?

yocto project‌ linux kernel #keras#opencv#package_deb in yocto
0 项奖励
回复
3 回复数

2,228 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Jarvis Crypter,

Keras and Tensor Flow are not supported on the NXP BSPs so you would need to do the porting yourself for which I would recommend the i.MX BSP Porting Guide available as part of the BSP documentation and the Yocto Project documentation.

Regards,

0 项奖励
回复

2,228 次查看
gaurangk
Contributor I

Hi,

Can't we use sensor flow meta layer available here http://layers.openembedded.org/layerindex/branch/master/layer/meta-tensorflow/.

Should it work or do I need to modify anything extra to add support of it?

0 项奖励
回复

2,228 次查看
maharajan
Contributor I

Hello,

Is this applicable to i.MX8 BSP as well. Do you not have Tensorflow or Keras support for i.MX8 as well? If yes, then are there any other Machine Learning or Deep Learning frameworks that NXP supports in its i.MX BSPs? 

Thanks

0 项奖励
回复