Building a custom kernel for NXP "Freescale i.MX8MQ EVK" board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Building a custom kernel for NXP "Freescale i.MX8MQ EVK" board

1,262 Views
ramesh_r
Contributor I

Hello,

I have a i.IMX8MQ NXP EVK. This currently boots up with linux kernel version 4.14.98-00063-gbcdaf61.

Can someone please help me download the linux kernel source for this board, build an image & boot up using that kernel? 

Thanks & Regards

Ramesh

iMX8MQ-EVK.jpg

0 Kudos
4 Replies

1,225 Views
ramesh_r
Contributor I

Ok, thanks.

0 Kudos

1,256 Views
igorpadykov
NXP Employee
NXP Employee

Hi ramesh_r

 

build steps can be found in Yocto Guide included in Documentation

for this release, sources are described in Table 5. i.MX Code Aurora Forum Distributed Repos

Release Notes.

https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.98_2.0.0_ga

All Linux documentation

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 Kudos

1,248 Views
ramesh_r
Contributor I

Thanks Igor,

I have another board, this is iMX6 EVK

Board: MX6SX SABRE SDB

This is currently running linux ver 4.9.88.

1) Need to download the ARM toolchain,

2) Download the linux kernel source

3) build an image

4) need to upgrade / flash the newly built image to boot up the board.

Could you also point me to the documentation to get the above listed items done as well for iMX6?

Thanks in advance. Attaching a picture & HW Info for reference.

==

cat /proc/cpuinfo
processor : 0
model name : ARMv7 Processor rev 10 (v7l)
BogoMIPS : 3.00
Features : half thumb fastmult vfp edsp neon vfpv3 tls vfpd32
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x2
CPU part : 0xc09
CPU revision : 10

Hardware : Freescale i.MX6 SoloX (Device Tree)
Revision : 0000
Serial : 0000000000000000

==


Regards

Ramesh

 iMX6SX_SABRE_SDB.jpg

0 Kudos

1,231 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ramesh

 

since this is new processor suggest to create new community thread for these questions.

 

Best regards
igor

0 Kudos