Hi
i'm following the "Freescale Yocto project User's guide" to build the image x11 on the i.XM 6quad sabre-sd but i'm having issues
I had multiple issues during the "bitbake fsl-image-x11" command that i managed to solved.
When i'm finally reaching the eand (task 4721/4748) i get this error multiple times:
ERROR: QA Issue: non debug package contains .debug directory: qt4-examples path /work/imx6qsabresd-poky-linux-gnueabi/qt4-x11-free/1_4.8.5-r0/packages-split/qt4-examples/usr/bin/qt4/examples/declarative/cppextensions/referenceexamples/extended/.obj/release-shared/.debug/qrc_extended.o
and at the end of it:
ERROR: QA run found fatal errors. Please consider fixing them.
ERROR: Function failed: do_package_qa
ERROR: Logfile of failure stored in: /mnt/Ubuntu/fsl-release-bsp/build-x11/tmp/work/imx6qsabresd-poky-linux-gnueabi/qt4-x11-free/1_4.8.5-r0/temp/log.do_package.2921
ERROR: Task 515 (/mnt/Ubuntu/fsl-release-bsp/sources/poky/meta/recipes-qt/qt4/qt4-x11-free_4.8.5.bb, do_package) failed with exit code '1'
I tried removing all the .o files concerned by hand, but this didn't solve the problem since they are created everytime.
I also tried some solutions found on the internet, like adding some lines in the bb files but this didn't work either.
It's been a week i'm trying to make this work, and i'm all out of ideas.
Thx by advance.
Ce message a été modifié par : Philippe Balleydier
解決済! 解決策の投稿を見る。
I'm not getting any answers on the mailing list.
for your information, i'm building the image on a ntfs partition and i had a lot of permission issues during the bitbake process. So I assume the problem comes from here.
I'm currently creating a ext2/3 partition to build the image on. I'll keep you updated.
Try posting to meta-fsl-arm mailing list.
I'm not getting any answers on the mailing list.
for your information, i'm building the image on a ntfs partition and i had a lot of permission issues during the bitbake process. So I assume the problem comes from here.
I'm currently creating a ext2/3 partition to build the image on. I'll keep you updated.
I did solve my problem
Thanks.
Phillippe,
I too have spent 1 week trying to figure this out. Can you explain what you did?
Thanks!
My problem was mainly due to permissions issues. I didn't mount my partition properly. I highly recommend to use Ubuntu 12.04 and to deploy your images on the main partition. This should work like a charm. If you have to mount a partition for some reasons (just like me), make sure your permissions are set correctly
** Modified original post, re-up thread **