HI
I am trying to build Android Images for imx6dl sabresd platform on ubuntu12.04LTS(64-bit OS) . Steps i followed are below:
[1] cd <enter into code directory>
[2] source build/envsetup.sh
[3] lunch sabresd_6dq-user
[4] make
After build, i checked build_sabresd_6dq_android.log to make sure that there does not exist any build error.But, i am getting like below scripts:
-----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
build/core/Makefile:32: warning: overriding commands for target `out/target/product/sabresd_6dq/system/etc/permissions/android.software.live_wallpaper.xml'
build/core/base_rules.mk:520: warning: ignoring old commands for target `out/target/product/sabresd_6dq/system/etc/permissions/android.software.live_wallpaper.xml'
No private recovery resources for TARGET_DEVICE sabresd_6dq
make: *** No rule to make target `kernel_imx/arch/arm/configs/imx6_android_defconfig', needed by `out/target/product/sabresd_6dq/.config'. Stop.
--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Please, help me to sort out this build error.
Thank You
Kapil Kumar
Solved! Go to Solution.
Hi Saurabh
I could able to build it now. Yes, you were right that "imx6_android_defconfig" is missing and not present in kernel_imx/arch/arm/configs.
Now, i am able to build it.
But, one more problem now i am getting . I put my SD-Card into the slot .(u-boot.bin, boot.img, system.img, recovery.img) ,i copied into card using dd utility. Afterthat, i tried booting the board, on hyperterminal
"init:untracked pid ...exited" // this message is coming continuously. and android is flashing on the display of the board.
Thank You
Kapil Kumar.
Hi Saurabh
But, one more problem now i am getting . I put my SD-Card into the slot .(u-boot.bin, boot.img, system.img, recovery.img) ,i copied into card using dd utility. Afterthat, i tried booting the board. on hyperterminal
"init:untracked pid ...exited" // this message is coming continuously. and android is flashing on the display of the sabresdb board.
Thank You.
Kapil Kumar
Hi Kapil
According to your Android build, it requires "imx6_android_defconfig"
Please check that file is available in arch/arm/configs/
While in above steps you are using " imx_v7_android_defconfig"
So go through "Android_User's_Guide.pdf"
Thanks
Saurabh
Hi Saurabh
I could able to build it now. Yes, you were right that "imx6_android_defconfig" is missing and not present in kernel_imx/arch/arm/configs.
Now, i am able to build it.
But, one more problem now i am getting . I put my SD-Card into the slot .(u-boot.bin, boot.img, system.img, recovery.img) ,i copied into card using dd utility. Afterthat, i tried booting the board, on hyperterminal
"init:untracked pid ...exited" // this message is coming continuously. and android is flashing on the display of the board.
Thank You
Kapil Kumar.
Kapil,
Are you still having problems?
Yes...
Hi Kapil,
Please check your kernel_imx folder is cloned correctly.
Error says that "imx6_android_defconfig" is missing in your kernel_imx folder.
Thanks
Saurabh
Hi Saurabh
How can i verify whether it has been cloned properly or not? I simply downloaded by following the steps given in the Android user guide.
if it has not been cloned properly, then, how i am able to build kernel? Actually, i tried building kernel by the steps outlined below, and i got uImage ready in the folder ~/kernel_imx/arch/arm/boot/uImage.
Steps:
[1]
make imx_v7_android_defconfig
[2]
make uImage LOADADDR=0x10008000
Thank You
Kapil Kumar.