Build failed : ERROR: lzop-native-1.03-r0 do_configure: configure failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build failed : ERROR: lzop-native-1.03-r0 do_configure: configure failed

Jump to solution
1,360 Views
oussamadjedidi
Contributor II

I'm building a QT image for the imx6sxsabresd under ubuntu 16.10 (I have to do it under this version for other os considerations) .

When the build reaches task 941 of 7410 :

I get : ERROR: lzop-native-1.03-r0 do_configure: configure failed
Log file attached.

Original Attachment has been moved to: Build.log.zip

Labels (3)
1 Solution
1,096 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Oussama DJEDIDI,

Are you still receiving this error?

I wasn’t able to find information about this specific error that may help. I understand you needing to use Ubuntu 16.10 but chances are that you may find troubles baking the BSP using a version newer than Ubuntu 14.04.

You may want to remove the package if it’s not indispensable for the image in question or otherwise try to fix the configuration mismatch, which may be tricky.

Regards,

View solution in original post

2 Replies
1,096 Views
oussamadjedidi
Contributor II

Thank you very much

0 Kudos
Reply
1,097 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Oussama DJEDIDI,

Are you still receiving this error?

I wasn’t able to find information about this specific error that may help. I understand you needing to use Ubuntu 16.10 but chances are that you may find troubles baking the BSP using a version newer than Ubuntu 14.04.

You may want to remove the package if it’s not indispensable for the image in question or otherwise try to fix the configuration mismatch, which may be tricky.

Regards,