Build failed : ERROR: lzop-native-1.03-r0 do_configure: configure failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build failed : ERROR: lzop-native-1.03-r0 do_configure: configure failed

ソリューションへジャンプ
2,206件の閲覧回数
oussamadjedidi
Contributor II

I'm building a QT image for the imx6sxsabresd under ubuntu 16.10 (I have to do it under this version for other os considerations) .

When the build reaches task 941 of 7410 :

I get : ERROR: lzop-native-1.03-r0 do_configure: configure failed
Log file attached.

Original Attachment has been moved to: Build.log.zip

ラベル(3)
タグ(3)
1 解決策
1,942件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Oussama DJEDIDI,

Are you still receiving this error?

I wasn’t able to find information about this specific error that may help. I understand you needing to use Ubuntu 16.10 but chances are that you may find troubles baking the BSP using a version newer than Ubuntu 14.04.

You may want to remove the package if it’s not indispensable for the image in question or otherwise try to fix the configuration mismatch, which may be tricky.

Regards,

元の投稿で解決策を見る

2 返答(返信)
1,942件の閲覧回数
oussamadjedidi
Contributor II

Thank you very much

0 件の賞賛
返信
1,943件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Oussama DJEDIDI,

Are you still receiving this error?

I wasn’t able to find information about this specific error that may help. I understand you needing to use Ubuntu 16.10 but chances are that you may find troubles baking the BSP using a version newer than Ubuntu 14.04.

You may want to remove the package if it’s not indispensable for the image in question or otherwise try to fix the configuration mismatch, which may be tricky.

Regards,