Build fail when set gst-fsl-plugins in ltib configuration.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build fail when set gst-fsl-plugins in ltib configuration.

Jump to solution
1,336 Views
hanseunglee
Contributor III

pastedImage_0.png

Hello.

I am going to set camera system in csi0 paraller port of i.mx6 sabresd borad .

I was set gst-fsl-plugins and compile.

=====================

Build path taken because: directory build,

checking if sources have been updated: no

Processing: libtermcap

========================

Processing: bash

==================

Processing: zlib

==================

Processing: net-tools

=======================

Processing: ethtool

=====================

Processing: wireless-tools

============================

Processing: iproute

=====================

Processing: i2c-tools

=======================

Processing: hotplug

=====================

Processing: glib2

===================

Processing: alsa-lib

======================

Processing: libxml2

=====================

Processing: udev

==================

Processing: dhcp

==================

Processing: liboil

====================

Processing: gstreamer-core

============================

Processing: gst-plugins-base

==============================

Processing: gst-plugins-good

==============================

Processing: firmware-imx

==========================

Processing: imx-lib

=====================

Processing: imx-vpu-lib

=========================

Processing: imx-test

======================

Build path taken because: directory build,

checking if sources have been updated: no

Processing: kobs-ng

=====================

Processing: wpa_supplicant

============================

Processing: libfslcodec

=========================

Build path taken because: no prebuilt rpm,

Testing network connectivity

OK GPP:

Try libfslcodec-3.0.7-2.tar.gz.md5 from the GPP

http://bitshrine.org/gpp/libfslcodec-3.0.7-2.tar.gz.md5:

09:31:51 ERROR 404: Not Found.

Try libfslcodec-3.0.7-2.tar.gz from the GPP

http://bitshrine.org/gpp/libfslcodec-3.0.7-2.tar.gz:

09:31:52 ERROR 404: Not Found.

Can't get: libfslcodec-3.0.7-2.tar.gz at ./ltib line 802.

f_buildrpms() returned an error, exiting

traceback:

main:572

Started: Fri Mar  4 09:31:10 2016

Ended:   Fri Mar  4 09:31:52 2016

Elapsed: 42 seconds

These packages failed to build:

libfslcodec

Build Failed

Exiting on error or interrupt

-----------------------------------------------------------------------------------------

How can i solve the problem?

0 Kudos
Reply
1 Solution
1,048 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please follow recommendations in the followoing documentation

http://www.nxp.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_MMDOCS&Parent_nodeId=1337699481071706...

http://www.nxp.com/webapp/Download?colCode=L3.0.101_4.1.1_MM_CODECS&appType=license&location=null&Pa...

Summary Page :
i.MX 6 Series Software and Development Tool|NXP

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,049 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please follow recommendations in the followoing documentation

http://www.nxp.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_MMDOCS&Parent_nodeId=1337699481071706...

http://www.nxp.com/webapp/Download?colCode=L3.0.101_4.1.1_MM_CODECS&appType=license&location=null&Pa...

Summary Page :
i.MX 6 Series Software and Development Tool|NXP

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply