Build error on IMX8MEVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build error on IMX8MEVK

1,453件の閲覧回数
sunnyvan
Contributor II

Dear all,

 I tried to follow the instruction https://www.nxp.com/docs/en/user-guide/i.MX_Yocto_Project_Useand i.MX_Yocto_Project_User's_Guide to build a imx8qevk image,I followed all the instruction from the beginning step by step,however,when i ran bitbake fsl-image-qt5-validation-imx,it gave errors as below:

van@ubuntu:~/imx-yocto-bsp/build-wayland$ bitbake fsl-image-qt5-validation-imx

NOTE: Your conf/bblayers.conf has been automatically updated.
NOTE: Your conf/bblayers.conf has been automatically updated.
WARNING: Host distribution "Ubuntu-16.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |###########################################################################################################| Time: 0:00:01
Loaded 3068 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.32.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-16.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mqevk"
DISTRO = "fsl-imx-wayland"
DISTRO_VERSION = "4.9.51-mx8-ga"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""
meta
meta-poky = "HEAD:8298428c032ec9bc5b514d0c194a16cf371475ea"
meta-oe
meta-multimedia = "HEAD:b40116cf457b88a2db14b86fda9627fb34d56ae6"
meta-freescale = "HEAD:05681fdf8298bb441c15135eae424c7601b07e98"
meta-freescale-3rdparty = "HEAD:e55167c3c2770c07a475342f99cc2a3a23fbfa0c"
meta-freescale-distro = "HEAD:cd5c7a2539f40004f74126e9fdf08254fd9a6390"
meta-bsp
meta-sdk = "HEAD:0649ff215e8f9b79ecd3b813d672547aa45c086b"
meta-browser = "HEAD:678706cb43fb8576ff7b88bfb612993b8542724d"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:b40116cf457b88a2db14b86fda9627fb34d56ae6"
meta-qt5 = "HEAD:ff073f04109900fc07bf81e2f1df63c626caf342"

Initialising tasks: 100% |######################################################################################################| Time: 0:00:11
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: binutils-cross-aarch64-2.27-r0 do_compile: oe_runmake failed
ERROR: binutils-cross-aarch64-2.27-r0 do_compile: Function failed: do_compile (log file is located at /home/van/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/binutils-cross-aarch64/2.27-r0/temp/log.do_compile.2719)
ERROR: Logfile of failure stored in: /home/van/imx-yocto-bsp/build-wayland/tmp/work/x86_64-linux/binutils-cross-aarch64/2.27-r0/temp/log.do_compile.2719

Attachments is log files,I changed the operating system version(Ubuntu 18.04,12.04),  but the compilation still failed.

How can I solve this problem? 

ラベル(1)
0 件の賞賛
返信
1 返信

1,208件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

I apologize for the delay.

Are you installing all the package that our guide says?

Furthermore, can you please try using Ubuntu 14.04. Also, instead of using the wayland distro, please try using the xwayland distro. I know that wayland is no longer supported by the i.MX8MQ.

Hope this can help you.

Best regards,

Diego.

0 件の賞賛
返信