Build Yocto for BSP 4.0.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build Yocto for BSP 4.0.0

ソリューションへジャンプ
2,437件の閲覧回数
MarcoSandrelli
Contributor III

Hi at all,

how can I build Yocto for iMX6 BSP 4.0.0? We have only one Yocto for all iMX6 platform like ubuntu?

Thanks!

ラベル(2)
0 件の賞賛
返信
1 解決策
2,074件の閲覧回数
LeonardoSandova
Specialist I

Actually the release number is 1.4 and I am not sure about the release dates. Subscribe to the mailing list to cehck latest status.

Leo

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,074件の閲覧回数
LeonardoSandova
Specialist I

I can not fully answer first question but after a BSP release using LTIB, Yocto moves quickly to be at the same level as ltib. In the near future, this won't be a problem because the building platform will only be Yocto. For the second question, the answer is yes,

Freescale Community BSP Release Notes 1.4a documentation

However, you need to specify the machine for each build, so there is no ONE image which boots every iMX.

Leo

2,074件の閲覧回数
MarcoSandrelli
Contributor III

Hi Leo,

Thank you very much for your answer,

a release date for Yocto BSP 4.0.0?

:smileyhappy:

0 件の賞賛
返信
2,075件の閲覧回数
LeonardoSandova
Specialist I

Actually the release number is 1.4 and I am not sure about the release dates. Subscribe to the mailing list to cehck latest status.

Leo

0 件の賞賛
返信