Build KK4.4.3 Android image:V8MediaQueryList.h: No such file or directory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build KK4.4.3 Android image:V8MediaQueryList.h: No such file or directory

2,531件の閲覧回数
albert_zhang
Contributor II

Today, when i try to build android image for i.mx6q-sd board, and i follow Android_User's_Guide but i didn't patch android_KK4.4.3_2.0.0-ga_omxplayer_source.tar.gz and android_KK4.4.3_2.0.0-ga_wfdsink_source.tar.gz packages. This is my command order after c_patch command:

1.source build/envsetup.sh

2.lunch sabresd_6dq-eng 

3.make

And then, i got a fatal error:external/chromium_org/third_party/WebKit/Source/core/css/MediaQueryListListener.cpp:23:30: fatal error: V8MediaQueryList.h: No such file or directory

I search this error on community but i didn't find the same problem.

Does anyone meet this? Hope give me some advice.

 

Thanks,

albert

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

1,466件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Albert,

The issue would be related that our GIT server where move to Code Aurora, here is the link

i.MX - Code Aurora 

0 件の賞賛
返信

1,466件の閲覧回数
albert_zhang
Contributor II

Hi jamesbone,

I see the link, but there are many repositories. I wanna build KK4.4.3_2.0.0 version for i.MX6Q-SD board but i get this error, I really don't know which repository, which branch and which version should i clone.I just follow Android_User's_Guide(KK4.4.3_2.0.0), should i repo again? Could you provide clone link?

Thanks,

albert

0 件の賞賛
返信