Bug: kernel hang when lcd resolution larger than 800x600 and HAB is enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bug: kernel hang when lcd resolution larger than 800x600 and HAB is enabled

1,253 Views
yunyangsihai
Contributor II

Dear all:

I trying to test the Secure Boot (HAB). And HAB is ok now.

iMX6UL + BSP4.1.15_1.0.0

1. But kernel will hang when lcd resolution is 1024x768 (larger than 800x600) and HAB is enabled.

2. kernel boot up sucessfully when lcd resolution is 800x600 (only resolution is changed) and HAB is enabled.

3. kernel always boot up successfully when HAB is not enabled.

Summary as follows:

LCD resolution HAB offHAB on
800*480okok
800*600okok
1024*768okfailed (kernel hang)
1280*800okfailed (kernel hang)

 

log file:

<HAB-enabled-1024x768-kernel-hang.txt> : HAB is enabled and lcd resolution is 1024x768, kernel will hang.

yunyangsihai_0-1632735387434.png

HAB-enabled-1024x768-kernel-hang.png

<HAB-enabled-800x600-kernel-ok.txt> : HAB is enabled and lcd resolution is 800x600, kernel boot up successfully.

yunyangsihai_1-1632735435882.png

HAB-enabled-800x600-kernel-ok.png

 

yunyangsihai_2-1632735476639.png

HAB-enabled-test-ok.png

0 Kudos
Reply
5 Replies

1,246 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yang

 

unfortunately L4.1.15 is not more supported as outdated, recommended to try with

latest linux and Code Signing Tool releases described on

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

https://www.nxp.com/design/software/embedded-software/i-mx-software:IMX-SW

 

Best regards
igor

0 Kudos
Reply

1,187 Views
yunyangsihai
Contributor II

1. This problem can also reproduced on latest Code Signing Tool releases cst-3.3.1

2. Upgrade to the latest Linux is so heavy work, it is impossible.

0 Kudos
Reply

1,241 Views
yunyangsihai
Contributor II

Thanks.

How can I know the Release Date and Support time of every BSP-version?

We will request support by sales.

0 Kudos
Reply

1,236 Views
igorpadykov
NXP Employee
NXP Employee

>How can I know the Release Date and Support time of every BSP-version?

 

release date is provided in Release Notes document included in each BSP package on below link,

support time is 1 year from release date.

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 Kudos
Reply

1,251 Views
yunyangsihai
Contributor II

dts file is "dh180_a6g2c-wifi-bt-128m.dts" ,as attached zip.

0 Kudos
Reply