Bug in busfreq driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bug in busfreq driver

ソリューションへジャンプ
2,088件の閲覧回数
maximkuk
Contributor III

Hello!

On our custom board (imx6d + lpddr2, pop-package) we faced with kernel panic after some tome of work. After some reserces I detected that busfreq causes this.

The thing is that before change ddr frequancy, driver (in function "update_lpddr2_freq_smp") compares new freq value with current and if they equals it returns 0. After that driver configures clock parents and if frequancies not configured before it (because update_lpddr2_freq_smp doesn't actually work) system crashes.

Some times in "update_lpddr2_freq_smp" curr_ddr_rate doesn't changes after previous call. Make it volatile not help. If not check curr_ddr_rate - all works perfect.

Why curr_ddr_rate doesn't change sometimes? And do we need curr_ddr_rate if all other work doings unconditionally?

ラベル(3)
0 件の賞賛
返信
1 解決策
1,764件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Maxim

please try ddr test and use nxp bsps described on below link

i.MX6/7 DDR Stress Test Tool V2.80 

i.MX Software|NXP 

https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.1.15_2.0.0_galinux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,765件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Maxim

please try ddr test and use nxp bsps described on below link

i.MX6/7 DDR Stress Test Tool V2.80 

i.MX Software|NXP 

https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.1.15_2.0.0_galinux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,764件の閲覧回数
maximkuk
Contributor III

Thank you for answer and useful links!

It looks like I found the same solution - update curr_ddr_rate before changing ddr frequency.

0 件の賞賛
返信