Bug in Vivante i.MX6 Wayland drivers when destroying windows

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bug in Vivante i.MX6 Wayland drivers when destroying windows

19,444 Views
cola
Contributor I

We are getting the following client-side crash with our compositor when destroying windows. Apparently, the proxy object is nullptr though it never shall be.

We are using SDK release 5.0.11.p8.4.

  1. Thread 2 (Thread 3662.3673):
  2. #0  wl_proxy_add_listener (proxy=0x0, implementation=0x74b621cc <gcsWL_FRAME_LISTENER>, data=data@entry=0x5e424d0c) at /usr/src/debug/wayland/1.9.0-r0/wayland-1.9.0/src/wayland-client.c:464
  3. No locals.
  4. #1  0x74b53544 in wl_callback_add_listener (data=0x5e424d0c, listener=0x74b621cc <gcsWL_FRAME_LISTENER>, wl_callback=<optimized out>) at /home/bamboo/automation/3.14.52-1.1.1/graphics_pkg/temp_build_dir/build-imx6qsabresd/tmp/sysroots/imx6qsabresd/usr/include/wayland-client-protocol.h:317
  5. No locals.
  6. #2  gcoOS_SetDisplayVirtualEx (Display=<optimized out>, Window=0x5e424c84, Context=0x5e424d0c, Surface=<optimized out>, Offset=0, X=0, Y=0) at gc_hal_user_wayland.c:1692
  7.         swapInterval = -1
  8.         ret = <optimized out>
  9.         i = <optimized out>
  10.         wl_window = 0x5e424c84
  11.         egl_buffer = 0x5e424d0c
  12.         wl_buffer = 0x5e457d40
  13.         display = 0x19d608
  14. #3  0x74a843ac in veglSetDisplayFlip (Display=Display@entry=0x19d6bc, Surface=<optimized out>, BackBuffer=BackBuffer@entry=0x5e4255dc) at gc_egl_platform.c:249
  15.         status = <optimized out>
  16. #4  0x74a7ec6c in veglSwapWorker (Display=0x19d6bc) at gc_egl_swap.c:741
  17.         display = 0x19d6bc
  18.         displayWorker = 0x5e4255cc
  19.         currWorker = 0x5e4255cc
  20.         bStop = 0
  21.         __user_ptr__ = <synthetic pointer>
  22. #5  0x75a4cf5c in start_thread (arg=0x65556440) at /usr/src/debug/glibc/2.24-r0/git/nptl/pthread_create.c:335
  23.         pd = 0x65556440
  24.         unwind_buf = {cancel_jmp_buf = {{jmp_buf = {2123239463, 1853849923, 1700095040, 2130704288, 0, 338, 0, 0, 2130704288, 1700093820, 0 <repeats 54 times>}, mask_was_saved = 0}}, priv = {pad = {0x0, 0x0, 0x0, 0x0}, data = {prev = 0x0, cleanup = 0x0, canceltype = 0}}}
  25.         not_first_call = <optimized out>
  26.         robust = <optimized out>
  27.         pagesize_m1 = <optimized out>
  28.         sp = <optimized out>
  29.         freesize = <optimized out>
  30.         __PRETTY_FUNCTION__ = "start_thread"
  31. #6  0x75d42408 in ?? () at ../sysdeps/unix/sysv/linux/arm/clone.S:86 from /opt/sdk/cebis/sysroots/cortexa9hf-neon-mel-linux-gnueabi/lib/libc.so.6
  32. No locals.
  33. Backtrace stopped: previous frame identical to this frame (corrupt stack?)
0 Kudos
Reply
29 Replies

3,518 Views
cphealy1
Senior Contributor I

As an alternative to a potentially improved Vivante driver, it is now possible to run the latest upstream Weston (4.0) with mainline kernel, libdrm, and Mesa.  There are optimizations in upstream Weston specifically for the Vivante GPU that result in very good performance on the i.MX6 when running with mainline kernel, libdrm, and Mesa.  (Mesa is what provides the opensource driver for the Vivante GPU in the i.MX6 when running a non NXP-BSP based kernel.)

I've been running with this stack for some time now and it works quite well.  It would require you move from whatever version of kernel you are currently running to Linux 4.16 though which may not be an option in your case.

0 Kudos
Reply

3,518 Views
jrtigerlee
Contributor III

Hi Chris ,

Do you have any guideline to porting weston 4.0 with mainline kernel can share with us?

0 Kudos
Reply

3,518 Views
cphealy1
Senior Contributor I

Hi Jrtiger,

There isn't really much in the context of "porting" it.  If you take stock Linux 4.16 (or newer) with stock libdrm 2.4.89 (or newer) with stock Mesa 18.0 and build stock Weston 4.0, you should have a working stack that just works.

In the kernel, libdrm, and Mesa, you need to make sure "etnaviv" is enabled.  (etnaviv is vivante spelled backwards....)

With this stack, LVDS and HDMI output should work correctly and the GPU will be used to accelerate Weston for compositing as well as the GPU being available for any applications that use OpenGL ES 2.0.  (Qt 5.10.1 is a good example of this.  It's will use OpenGL ES 2.0 for acceleration.)

With a 1080p display and the i.MX6qp, many applications operate at 60fps. 

With the mainline stack, not only is the GPU properly supported but the VPU (Video decoder) also just works.  You'll want to have gstreamer 1.14.  With this combination, no special NXP plugins are required and 1080p video playback will be ~1% CPU load.

Regards,

Chris

0 Kudos
Reply

3,518 Views
jrtigerlee
Contributor III

Hi Chris ,

I was using Yocto morty to build system, and will try to use Yocto rocko or sumo to create this new stuff.

Thanks for your experience sharing.

I'll glad that if you have more GPU benchmark sharing , like glmark2 score in 1080P resolution.

0 Kudos
Reply

3,518 Views
cphealy1
Senior Contributor I

Hi Jrtiger,

Below is the output of glmark2-es2-wayland.  The display is 1920x1080.  The SoC is the i.MX6qp and it's running Weston (Wayland compositor).  Performance is a bit lower than should be expected as our HW platform has the GPU shader clock reduced from the default 720Mhz to 594Mhz.  Within the next few months, I expect the framerate going up substantially as there is a compositor bypass feature being worked on for Weston that gets turned on when running an application fullscreen.  (Composition is not needed when there's only one application on the screen.)

root@RDU2:~ glmark2-es2-wayland --fullscreen
=======================================================
    glmark2 2014.03
=======================================================
    OpenGL Information
    GL_VENDOR:     etnaviv
    GL_RENDERER:   Vivante GC3000 rev 5450
    GL_VERSION:    OpenGL ES 2.0 Mesa 18.0.0.20180404-1
=======================================================
[build] use-vbo=false: FPS: 295 FrameTime: 3.390 ms
[build] use-vbo=true: FPS: 360 FrameTime: 2.778 ms
[texture] texture-filter=nearest: FPS: 333 FrameTime: 3.003 ms
[texture] texture-filter=linear: FPS: 331 FrameTime: 3.021 ms
[texture] texture-filter=mipmap: FPS: 322 FrameTime: 3.106 ms
[shading] shading=gouraud: FPS: 267 FrameTime: 3.745 ms
[shading] shading=blinn-phong-inf: FPS: 191 FrameTime: 5.236 ms
[shading] shading=phong: FPS: 129 FrameTime: 7.752 ms
[shading] shading=cel: FPS: 95 FrameTime: 10.526 ms
[bump] bump-render=high-poly: FPS: 168 FrameTime: 5.952 ms
[bump] bump-render=normals: FPS: 217 FrameTime: 4.608 ms
[bump] bump-render=height: FPS: 164 FrameTime: 6.098 ms
libpng warning: iCCP: known incorrect sRGB profile
[effect2d] kernel=0,1,0;1,-4,1;0,1,0;: FPS: 46 FrameTime: 21.739 ms
libpng warning: iCCP: known incorrect sRGB profile
[effect2d] kernel=1,1,1,1,1;1,1,1,1,1;1,1,1,1,1;: FPS: 12 FrameTime: 83.333 ms
[pulsar] light=false:quads=5:texture=false: FPS: 205 FrameTime: 4.878 ms
libpng warning: iCCP: known incorrect sRGB profile
[desktop] blur-radius=5:effect=blur:passes=1:separable=true:windows=4: FPS: 26 FrameTime: 38.462 ms
libpng warning: iCCP: known incorrect sRGB profile
[desktop] effect=shadow:windows=4: FPS: 96 FrameTime: 10.417 ms
[buffer] columns=200:interleave=false:update-dispersion=0.9:update-fraction=0.5:update-method=map: FPS: 46 FrameTime: 21.739 ms
[buffer] columns=200:interleave=false:update-dispersion=0.9:update-fraction=0.5:update-method=subdata: FPS: 45 FrameTime: 22.222 ms
[buffer] columns=200:interleave=true:update-dispersion=0.9:update-fraction=0.5:update-method=map: FPS: 58 FrameTime: 17.241 ms
[ideas] speed=duration: FPS: 162 FrameTime: 6.173 ms
[jellyfish] <default>: FPS: 58 FrameTime: 17.241 ms
[terrain] <default>: FPS: 4 FrameTime: 250.000 ms
[shadow] <default>: FPS: 132 FrameTime: 7.576 ms
[refract] <default>: FPS: 20 FrameTime: 50.000 ms
[conditionals] fragment-steps=0:vertex-steps=0: FPS: 243 FrameTime: 4.115 ms
[conditionals] fragment-steps=5:vertex-steps=0: FPS: 63 FrameTime: 15.873 ms
[conditionals] fragment-steps=0:vertex-steps=5: FPS: 231 FrameTime: 4.329 ms
[function] fragment-complexity=low:fragment-steps=5: FPS: 135 FrameTime: 7.407 ms
[function] fragment-complexity=medium:fragment-steps=5: FPS: 64 FrameTime: 15.625 ms
[loop] fragment-loop=false:fragment-steps=5:vertex-steps=5: FPS: 132 FrameTime: 7.576 ms
[loop] fragment-steps=5:fragment-uniform=false:vertex-steps=5: FPS: 116 FrameTime: 8.621 ms
[loop] fragment-steps=5:fragment-uniform=true:vertex-steps=5: FPS: 60 FrameTime: 16.667 ms
=======================================================
                                  glmark2 Score: 146
=======================================================

0 Kudos
Reply

3,518 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Andreas,

Could you provide your test? I can not reproduced it.

0 Kudos
Reply

3,518 Views
cola
Contributor I

Hi, I created a small test case and put it on GitHub:

GitHub - cordlandwehr/imx6_testcase_wayland-client-crash: Testcase for https://community.nxp.com/thr... 

Please see the include README.md for how to reproduce the bug.

0 Kudos
Reply

3,517 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Andreas,

I believe there are some bugs fix for segfault and crashes in most recent driver.  Could you try the attached most recent gpu 5.x p8 driver to see if your issue is fixed.

0 Kudos
Reply

3,517 Views
sanjeevsharma
Contributor IV

Dear Bio_TICFSl,

We have tried with 5.0.11.p8.6 & v6.2.2.p0 Vivante gpu driver version and also tried wayland v1.11.1 but Crash is still observed. if you look at the application code GitHub - cordlandwehr/imx6_testcase_wayland-client-crash: Testcase for https://community.nxp.com/thr... 

thread 2 looks like it's about to destroy the EGLSurface for this wl_surface which already got destroyed. So the question is why is this wl_surface destroyed before its EGLSurface is destroyed.

0 Kudos
Reply