Hello supporters,
At the very bottom of fsl_flexcan.c there is this:
#if defined(FLEXCAN2)
void CAN_FD2_DriverIRQHandler(void)
{
assert(NULL != s_flexcanHandle[2]);
s_flexcanIsr(FLEXCAN1, s_flexcanHandle[2]);
SDK_ISR_EXIT_BARRIER;
}
#endif
I think there is a mix-up between FLEXCAN1 and FLEXCAN2, higlighted in red. I'd appreciate your confirmation.
Thank you.
Best regards,
--
Thierry-
Finally fixed in the recent SDK 2.14.0. Thank you guys.
--
Thierry-
I just downloaded SDK_2_13_0_MIMX8ML8xxxKZ (latest & greatest 01.2023) and the reported bug is still present! I wonder how this driver is tested at NXP!?
The SDK where the bug initially showed up is version 2.9. I double-checked that the bug is still present in the latest version 2.11.1, archive file SDK_2.11.1_MIMX8ML8xxxLZ.zip. Please see file SDK_2_11_1_MIMX8ML8xxxLZ\devices\MIMX8ML8\drivers\fsl_flexcan.c, line 4638.
The device is an i.MX8M-Plus. The reported bug is believed to be board-independent. Just for your reference, the board is a BoundaryDevices SoM with a custom carrier.
Best regards,
--
Thierry-
Can you please clarify which board and device are you using? And the SDK version