BroadR-Reach support for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BroadR-Reach support for i.MX6

2,167 Views
_at
Contributor III

Hi,

I am working on a i.MX6. I need to give support BroadR-reach ethernet.

i.MX6 FEC is configured to communicate with BroadR-Reach PHY using MII.

Can anybody provide details about how actually BroadR-reach will works with i.MX6?

-Ankit.

Labels (2)
Tags (3)
5 Replies

1,233 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ankit

one can look at AVB software for

SABRE-AI-CPU2 board, which may connect enet card with BCM89810

SABRE-2|Automotive-Infotainment|i.MX6|Freescale

AVB.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,233 Views
_at
Contributor III

But status show:: Freescale's Audio Video Bridging Software is available for Evaluation. Development package will be available for order in Q3 quarter of 2015.

Do we have support for BCM89810? From where i can find the details ?

0 Kudos
Reply

1,233 Views
_at
Contributor III

Basically, i want to understand configuration/Initialization, Link Up/Down of BCM89810 with MAC.

0 Kudos
Reply

1,233 Views
AlbertH
Contributor II

Hello Ankit Patel,

Did you get the answer for this? I have the same question actively.

Thanks,

Albert

1,233 Views
_at
Contributor III

Any suggestion or response helpful to us ?

0 Kudos
Reply